Archive files
Click the
Archive Files
option to view archived system statistics.
FactoryTalk Historian ME stores your data in archives, which are the files that hold FactoryTalk Historian ME data. Archive files are fixed which means that they are always the same size, regardless of how much data they contain.
The archive receiving current data is called the
primary archive
. When the primary archive becomes full, an archive shift occurs, and the next available archive becomes the new primary archive. When the primary archive is being backed up, you cannot modify that archive or the Point database.Each archive file contains events for a time period specified by the archive start time and end time. The archive files on each FactoryTalk Historian ME server should cover all-time ranges, without overlapping time ranges or gaps in time. A list of archive files stored on FactoryTalk Historian ME is displayed by default when you select the
Archive Files
option.The
Archive Files
section displays the following information:Item | Description |
|---|---|
Archive File | The archive file name, which includes the full path. |
Status | The archive status displays one of the following:
|
Size (MB) | The archive file size in megabytes. |
Start Time | The time that data was first written to the archive file. |
End Time | The time that data was last written to the archive file. |
Lifetime | The archive file age in days, hours, minutes, and seconds. |
Last Modified Time | The last time and date the archive file was modified. |
Backup Time | The last time and date the archive file was backed up. Never indicates that the file has never been backed up. |
State | The state of the file:
|
Type | Indicates the type of file, which is always Fixed size . |
Write Flag | Specifies if a file is writable or read-only. |
Shift Flag | Specifies if a file is shiftable or not shiftable. |
Add Rate/Hour | The rate at which files are added to the archive per hour. |
% Full | The percentage of the archive that is being used. |
Annotations | The size in bytes of the annotation file associated with the archive file. |
Annotation File Size | The size in megabytes of the annotation file associated with the archive file. |
Shift Prediction | The target archive or the predicted shift time. |
Primary Offset | The number that indicates the number of primary archive records in use. |
Overflow Offset | The number that indicates the number of overflow records in use. |
Record Size | The record size for each archive record. |
Version | The version of the archive header. |
# | The archive number used by FactoryTalk Historian ME. |
Provide Feedback