Snapshot and archive
Click the
Snapshot and Archive
option to view the current FactoryTalk Historian ME snapshot and archive statistics.
The
Snapshot And Archive
section displays the following information:Item | Description |
|---|---|
Type | The snapshot or archive file type. |
Counter | The performance counter. For details, see Snapshot and archive counters. |
Value | The current snapshot and/or archive value. |
Change | The value change between updates. |
Provide Feedback