Install FactoryTalk Historian ME Client Tools
The FactoryTalk Historian ME Client Tools are a set of the following tools:
- FactoryTalk Historian ME Management
- FactoryTalk Historian ME Rule Editor
- FactoryTalk Historian ME Logix Designer Module Profile
The Client Tools are available on the FactoryTalk Historian ME installation DVD and as a download package on the Rockwell Automation Product Compatibility and Download Center website.
TIP:
If you download the Client Tools from the Rockwell Automation Product Compatibility and Download Center website and cannot extract the content of the package, check the length of the path to the directory to which you want to extract the package. If the length of the path to the directory is longer than 116 characters, you will not be able to extract the package to this location.
Provide Feedback