Install FactoryTalk Historian ME Logix Designer Module Profile
FactoryTalk Historian ME can be configured to communicate with a ControlLogix controller through the FactoryTalk Historian ME Logix Designer Module Profile.
TIP:
Install the Module Profile on the computer with
RSLogix 5000®
or Studio 5000 installed.To install the Module Profile
- Run the FactoryTalk Historian ME Client Tools DVD.The installation wizard appears.
- ClickInstall FactoryTalk Historian ME Client Tools>Install FactoryTalk Historian ME Logix Designer Module Profile.The Logix Designer Module Profile installation wizard appears.
- Follow the on-screen instructions to complete the process.
Provide Feedback