(optional) Install FactoryTalk Historian SE patch
If you want to integrate your
FactoryTalk Historian ME
with FactoryTalk Historian SE
2.1, you need to install the FactoryTalk Historian SE
patch. Once installed, FactoryTalk Historian ME
can work with FactoryTalk Historian SE
to collect, store, analyze, and visualize data using reporting tools such as time-series trends, bar charts, pie charts, pareto, and tabular trends.The
FactoryTalk Historian SE
patch must be installed on the FactoryTalk Directory
and any other computer that will be administering the FactoryTalk Historian ME
module through the FactoryTalk Administration Console
.The patch is not necessary for machines with
FactoryTalk Historian SE
2.2 or newer.You can download the
FactoryTalk Historian SE
patch from the Rockwell Automation
Knowledgebase page.Provide Feedback