Install FactoryTalk Historian ME Rule Editor

The Rule Editor allows you to create and edit user-defined rules for the point discovery process. The selections you make in the dialog box are automatically written to this file. The data points matching these rules are found and added to the FactoryTalk Historian server. You can upload the rule file to FactoryTalk Historian ME using the FactoryTalk Historian ME Upload Manager feature.
To install the Rule Editor
  1. Run the FactoryTalk Historian ME Client Tools DVD.
    The installation wizard appears.
  2. Click
    Install FactoryTalk Historian ME Client Tools
    >
    Install FactoryTalk Historian ME Rule Editor
    .
    The FactoryTalk Historian ME Rule Editor installation wizard appears.
  3. Follow the on-screen instructions to complete the process.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal