Overlay object
The Overlay object represents a trend overlay. An overlay is a captured snapshot added to a trend object and placed over a current trend display.
Set up overlays by using the Overlay object properties or the Overlays tab on the Trend Properties dialog box.
Use the
Item
method of the Overlays collection to get a reference to an Overlay object.The Overlay object provides the following properties and constants:
Provide Feedback