UseDefaultStartTime property

If the Anchor property is set to Time, returns or sets the UseDefaultStartTime property uses the default time or the value in the StartTime property. Read/write. Boolean.
The default start time is the time at the left-most side of the trend chart, when the chart is first brought up at runtime.
Syntax
overlay
.
DefaultStartTime
[
= value
]
where
overlay
- is an Overlay object, or an expression that evaluates to an Overlay object.
value - is a Boolean value that determines which start time is used.
  • True
    . Uses the default time
  • False
    . Uses the value from the StartTime property
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal