Example: StartTime and UseDefaultStartTime properties
Private Sub SetStartTime() ' Add an overlay to the overlays collection Trend1.Overlays.Add ("Overlay1") ' Overlay must be anchored by time to use the StartTime property Trend1.Overlays.Item(1).AnchorType = rstOverlayAnchorTypeTime Trend1.Overlays.Item(1).StartTime = #10/25/99 2:25:00 PM# ' Use the value from the StartTime property, not the default value Trend1.Overlays.Item(1).UseDefaultStartTime = False End Sub
Provide Feedback