StartTime property for Overlay object

Returns or sets or returns the start time. Read/write. DATE.
The earliest data in the overlay is anchored to when the Anchor property is set to rstTime.
Syntax
overlay
.
StartTime
[
= date
]
where
overlay
- is an Overlay object, or an expression that evaluates to an Overlay object.
date
- is a parameter of the type Date that specifies the start time for the data anchored to the overlay.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal