Wedge object

The Wedge object represents the intrinsic wedge object. It is not a creatable object. Wedge objects are accessible through an Elements collection.
The object-specific properties for the Wedge object are merged with the Element object's properties. This extended object is what the user will see when directly accessing the object from VBA using the object's name.
Properties
Methods
Constants
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal