gfxPatternStyleConstants
The following constants can be returned or set by the PatternStyle property.
gfxPatternStyleNone
– no patterngfxPatternStyleDots –
dot patterngfxPatternStyleChecks
– check patterngfxPatternStyleSmallBoxes
– small box patterngfxPatternStyleMediumBoxes
– medium box patterngfxPatternStyleLargeBoxes
– large box patterngfxPatternStyleVLines
– vertical line patterngfxPatternStyleWideVLines
– wide vertical line patterngfxPatternStyleHLines
– horizontal line patterngfxPatternStyleWideHLines
– wide horizontal line patterngfxPatternStyleRDiagonal
– right diagonal line patterngfxPatternStyleWideRDiagonal
– wide right diagonal line patterngfxPatternStyleLDiagonal
– left diagonal line patterngfxPatternStyleWideLDiagonal
– wide left diagonal line patterngfxPatternStyleHatch
– cross hatch patterngfxPatternStyleBricks
– brick patterngfxPatternStyleOvals
– oval patterngfxPatternStyleDiamonds
– diamond patterngfxPatternStyleScales
– scale patterngfxPatternStyleWaves
– wave patternProvide Feedback