PatternStyle property

Returns or sets the pattern used to fill a shape. Read/write. Constant.
Syntax
object
.
PatternStyle
[ =
value
]
where
object
– is the name of a graphic element or an expression that evaluates to a graphic element.
value
– is a constant of the type gfxPatternStyleConstants that specifies the style for the pattern.
Remarks
For the Button object, this property applies only to the Up state.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal