PatternColor property
Returns or sets the color used for the lines in the pattern. Read/write. OLE_COLOR.
OLE_COLOR is a type definition that resolves to a Long.
Syntax
object
.PatternColor
[ = value]where
object
– is the name of a graphic element or an expression that evaluates to a graphic element.value
– is an RGB color value that specifies the color of the lines for the object.Remarks
For the Button object, this property applies only to the Up state.
Provide Feedback