ToolTipText property

Returns or sets the text that is displayed when the mouse pauses on an object at runtime. Read/write. String.
If the tooltip text is changed while the tool tip is being displayed, the text that is shown does not change until the tool tip is canceled and redisplayed.
Syntax
element
.
ToolTipText
[ =
string
]
where
element
– is the name of a graphic element object or an expression that evaluates to a graphic element object.
string
– is the text that is to be displayed in the tool tip for the element.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal