RoundedRectangle object

The RoundedRectangle object represents the intrinsic rounded rectangle object. It is not a creatable object. RoundedRectangle objects are accessible through an Elements collection.
The object-specific properties for the RoundedRectangle object are merged with the Element object's properties. This extended object is what the user will see when directly accessing the object from VBA using the object's name.
Properties
Methods
Constants
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal