Polyline object
The Polyline object represents the intrinsic polyline object. It is not a creatable object. Polyline objects are accessible through an Elements collection.
The object-specific properties for the Polyline object are merged with the Element object's properties. This extended object is what the user will see when directly accessing the object from VBA using the object's name.
Properties
Methods
Constants
Provide Feedback