Polygon object
The Polygon object represents the intrinsic polygon object. It is not a creatable object. Polygon objects are accessible through an Elements collection.
The object-specific properties for the Polygon object are merged with the Element object's properties. This extended object is what the user will see when directly accessing the object from VBA using the object's name.
Remarks
Use the Polygon object in VBA code to interact with objects drawn with the Rectangle tool from the FactoryTalk View Graphics editor.
Properties
Methods
Constants
Provide Feedback