Freehand object
The Freehand object represents the intrinsic freehand object. It is not a creatable object.
Freehand objects are accessible through an Elements collection.
The object-specific properties for the Freehand object are merged with the Element object's properties. This extended object is what the user sees when directly accessing the object from VBA using the object's name.
Properties
Methods
Constants
Provide Feedback