Ellipse object

The Ellipse object represents the intrinsic ellipse object. It is not a creatable object. Ellipse objects are accessible through an Elements collection.
The object-specific properties for the Ellipse object are merged with the Element object's properties. This extended object is what the user sees when directly accessing the object from VBA using the object's name.
Properties
Methods
Constants
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal