Arrow object

The Arrow object represents the intrinsic arrow object. It is not a creatable object. Arrow objects are accessible through an Elements collection.
The object-specific properties for the Arrow object are merged with the Element object's properties. This extended object is what the user sees when directly accessing the object from VBA using the object's name.
Properties
Methods
Constants
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal