Arc object
The Arc object represents the intrinsic arc object. It is not a creatable object. Arc objects are accessible through an Elements collection.
The object-specific properties for the Arc object are merged with the Element object's properties. This extended object is what the user sees when directly accessing the object from VBA using the object's name.
Properties
Methods
Constants
Provide Feedback