Using XY Plot objects

You can use XY Plot to query data and plot it on a graphical display.
Use the XY Plot objects to:
  • See the relationship between the values of two tags (tag pair) over a historical period, a pre-set period, and in real-time. When plotted, this relationship is referred to as a trace.
  • Easily identify the boundaries that define "normal" conditions for a trace, by adding user-defined shapes.
  • Determine whether the value of a tag is outside of a defined boundary.
  • Display and compare multiple tags or traces concurrently.
  • Manipulate the data in a variety of ways, including panning, zooming, and scaling after you have added tags.
The supported data sources include
Live Data, FactoryTalk View SE data logs, FactoryTalk View SE DataLogPro, FactoryTalk Historian, FactoryTalk Historian Asset Framework, and OSIsoft PI Server
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal