Create an XY Plot object

Create an XY Plot object to show one set of tag values versus another set of tag values. This allows an operator to see the relationship between two sets of data over time.
The supported data sources include
Live Data, FactoryTalk View SE data logs, FactoryTalk View SE DataLogPro, FactoryTalk Historian, FactoryTalk Historian Asset Framework, and OSIsoft PI Server
.
To create an XY Plot object
  1. In the Toolbox, select
    XY Plot
    .
  2. Drag the mouse to create a box approximately the size the XY Plot chart is to be.
  3. On the
    General
    tab, specify the general runtime options.
  4. On the
    Common
    tab, specify the common properties such as size and positions.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal