Use events

An event is an action that is triggered by the evaluation of the expression associated with it. The action can be any
FactoryTalk View SE
command or macro. When the expression changes from False on the previous evaluation to True on the current evaluation, the action is triggered. An expression can be a tag name or it can be an equation made up of tag names, mathematical and logical operations, special functions, and If-Then-Else logic.
An events file consists of a number of events and a maximum update rate for them. At runtime, multiple events files can be active at once. You can run a maximum of 20 events files at one time, each containing up to 1000 events.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal