Specify a maximum update rate for an events file
The maximum update rate is the fastest rate, at which any event expression in an events component can be updated. The maximum update rate also determines the fastest rate, at which data servers can send changes in tag values.
Set a maximum update rate separately, for each event component you create.
Set the update rate as fast as, or faster than, the rate, at which the values of tags used in the expressions, change, unless it is desirable to miss changes in tag values.
The default maximum update rate for an events file is 1 second. When this time period elapses,
FactoryTalk View SE
updates the expressions that contain tags with values that have changed. You can change this in the Event Setup
dialog box that is available from the Setup
menu in the Events
editor.Provide Feedback