Create an events file
Use the
Events
editor to create an events file.By default, all events in an events file are updated every second (1 second). Use the
Event Setup
dialog box to change the maximum update rate.To create an events file:
- In.FactoryTalk View Studio, in the Explorer windows, navigate toLogic and Control, right-clickEventsand selectNew
- In theEventseditor, define the events for a file.
- From the menu, selectSetup>Event Setup.
- In theEvent Setupdialog box, select a maximum update rate and edit the description for the current events file, and clickOK.
- From the menu, selectFile>Save. Specify a file name when you are promoted to.
Provide Feedback