Edit an Events file
Use the Events editor to edit an Events file.
In addition to changing the action, enabled/disabled status, description and expression for an individual event, you can also add and delete events, and change the evaluation specifications for the Events file.
To edit an Events file:
- InFactoryTalk View SE, in the Explorer window, double-clickLogic and Control>Events.
- In the list of existing Events files, double-click the file you intend to edit.
- In the Events editor, make the changes in the form section of the editor and then clickAcceptto confirm them.
- ClickFile>Save.
Provide Feedback