Explorer window
The main tool for working in
FactoryTalk View Studio
. Provides access to the editors that you use to set up an application and create its components.When you open an application in
FactoryTalk View Studio
, the Explorer window is docked on the left-hand side of the main window beside the workspace.The Explorer window displays the
FactoryTalk Directory
icon at the top, and at the next level down, the FactoryTalk View
application folder and the System
folder.The
FactoryTalk View
application folder contains the editors and components you use to develop an application. In the System
folder, you use FactoryTalk Security
to specify which users, groups and computers have access to which resources in the system.Provide Feedback