Rename a component
When you rename a component, the component name and its path can take up to 256 characters.
Names for the following
FactoryTalk View Studio
components do not support extended ASCII characters or Unicode characters: applications, areas, HMI servers, data servers, HMI tags, FactoryTalk Linx
shortcuts, FactoryTalk View Studio
application files (SED files), and all FactoryTalk View
application components, including graphic displays, parameter files, macro files, events files, derived tag files, and data log files.
TIP:
To rename an application, use the
Application Manager
tool. For more information, see Application Manager Help.To rename a component:
- InFactoryTalk View Studio, in the Explorer window, right-click the component and selectRename.
- In theRenamedialog box, type the new name and clickOK.
Provide Feedback