Deploy a network distributed application

Deploy a network distributed application from the development computers to the production environment where it will run in a live setting.
To deploy a network distributed application
  1. On the development computer, use
    FactoryTalk View SE
    Application Manager to back up the application that FactoryTalk Network Directory requires.
  2. Use
    FactoryTalk View SE
    Application Manager to restore the application.
  3. After restoring RSLinx data servers in the application, renew or verify the topics, shortcuts, and device paths associated with each data server, as needed.
  4. After restoring the application, open the HMI server properties dialog box in
    FactoryTalk View Studio
    to verify the HMI server settings and set up additional HMI server properties as needed.
  5. If you have already set up
    FactoryTalk View SE
    client files for the application, copy the files to their new host computers. You do not have to modify the files after copying them. You can also create new
    FactoryTalk View SE
    clients using the
    FactoryTalk View SE
    Client Wizard.
  6. After deploying the application, run the deployed FactoryTalk View SE clients and test the application.
Remarks
  • All computers that take part in a network distributed application, including those that host a
    FactoryTalk View SE
    server or client, must point to the same
    FactoryTalk Directory
    computer. To do this, run the
    FactoryTalk Directory
    Server Location utility and specify the name of the
    FactoryTalk Directory
    computer, for each computer.
  • To use the FactoryTalk Directory Server Location Utility, you must sign in as a user with administrative privileges at the Network Directory and in Windows, on the computer where the utility is running.
  • For detailed information about completing the steps below, see Chapter 6 in the
    FactoryTalk View Site Edition User's Guide
    . For information about installing the FactoryTalk View Site Edition software, see the
    FactoryTalk View Site Edition Installation Guide
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal