FactoryTalk Directory
FactoryTalk Directory
enables the parts of an application to locate each other on a
computer or on the network. FactoryTalk Security
provides security for the resources
managed by FactoryTalk Directory
. You can set up FactoryTalk Security
to
restrict such things as who can open, modify, and delete an application or area, and who has
access to the FactoryTalk Directory
from which computers. For example, to access
graphic displays on an HMI server in the application, HMI clients use FactoryTalk Directory
to find out which computer on the network is hosting the HMI
server.FactoryTalk Directory
also stores the information about which users and computers
are allowed access to the various parts of a control system if you have used FactoryTalk
Security, to secure access to the resources that FactoryTalk Directory
manages.In a network system, if
FactoryTalk Directory
becomes unavailable while an
application is running, the application will continue to run correctly. For example, the FactoryTalk View SE
client will be able to read and write values, acknowledge alarms,
and open and close displays because a copy of the information provided by FactoryTalk Directory
is stored locally on each computer that is connected to the FactoryTalk Directory
computer. However, while FactoryTalk Directory
is
unavailable, you cannot modify an application's structure; for example, you cannot add or
edit an area, a data server, or an HMI server.If you are installing
FactoryTalk Services Platform
on a computer for the first time with the
standard FactoryTalk Directory mode:- In theFactoryTalkLocal Directory, all users have full access to the directory and toFactoryTalk View.
- In theFactoryTalkNetwork Directory, all users that are members of theWindows Administratorgroup on any local computer that is connected to theFactoryTalkNetwork Directory, will have full access to the directory and toFactoryTalk View.
If you are upgrading an existing
FactoryTalk
system that is earlier than
version 5.10, whatever security you previously set up will continue to be in effect.When you create a
FactoryTalk View SE
application, the user groups Windows
Administrators
and Administrators
are created in the FactoryTalk Directory
. Also, the group account All Users
is added automatically to the FactoryTalk View
Runtime Security accounts. By default, the All Users
group is granted all FactoryTalk View SE
runtime security codes (A - P), and all FactoryTalk Security
actions at the root directory node.
TIP:
The
FactoryTalk Directory
server must not be installed on the same computer as the
domain controller for the network.All the computers participating in a distributed application share a common
FactoryTalk Directory
located on a network computer.For more information about , or the
or the
FactoryTalk Directory
in FactoryTalk View
, see
Chapter 4 in the FactoryTalk View
Site Edition User's GuideFactoryTalk Services Platform Help
. For more information about FactoryTalk Security
in FactoryTalk View
, see Chapter 5 in the FactoryTalk View
Site Edition User's GuideFactoryTalk Services
Platform Help
.Provide Feedback