Copy a SE Client configuration file

The FactoryTalk View SE Client configuration files have the file extension .cli. The files are stored in the folder C:\Users\Public\Public Documents\RSView Enterprise\SE\Client.
To move a configuration file from one computer to another:
  1. On the source computer, locate and copy the
    .cli
    file you plan to move.
  2. On the target computer, locate the
    Client
    folder as specified above, and paste the
    .cli
    file into it.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal