Draw a line
You can use the
Line
option on the Objects
menu to draw lines as you would with a pen on paper.To draw a straight line:
- InFactoryTalk View Studio, in theGraphicseditor, selectObjects>Drawing>Line.
- Drag the tool from the beginning to end point to create the line you want.TIP:To draw only horizontal or vertical (not diagonal) lines, pressCtrlas you drag the tool.
- In theLine Propertiesdialog box, change the styles if needed.
- When the object is complete, draw another object. You can also click to finish drawing with the tool.
Provide Feedback