Sample HTML code
These samples provide examples of the HTML code along with screen shots of the code as it
appears with the Client.
e
Procedure
IMPORTANT:
The script code provided in these sections is intended only as examples. Any negative results due to using this script code are assumed by the user of this code.
The examples include control steps with:
- Operator instructions (see Control step with operator instructions)
- Operator instructions and Batch-specific data (see Control step with report data)
- Report data entry fields of all data types (see Control step with step verification)
- Non-specific web content (see Control step with other web content)eProcedure
Provide Feedback