Control step with confirmation

This example contains an input for a report value — the report is configured to require confirmation if the value is outside the High or Low limits. You can enter a comment, if desired.
ePro_client_confirm_value_dialog_box
<HTML>
<HEAD>
</HEAD>
<BODY LANG="EN-US" STYLE="tab-interval:.5in">
<FORM METHOD="Post" ENCTYPE="application/x-www-form-urlencoded">
Enter a value for REPORT_1: <INPUT TYPE="text" NAME="REPORT_1" HLConfirm="True" HLComment="True">
</FORM>
</BODY>
</HTML>
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal