Control step with step verification
This example uses a signature template called StepSig, which requires one signature.

<form>Record final amount of Sugar added to batch in<sop>UNIT</sop>: <input name="ACTUAL_AMOUNT" size="20" type="text"> <sop>ACTUAL_AMOUNT.eu</sop><br /><br />Note: Initial target amout for delivery was <sop>ADD_AMOUNT</sop> <sop>ADD_AMOUNT.eu</sop><br /><br/ >Press <b>OK</b> to continue.<sop>VerificationSig=StepSig</sop> </form>
Provide Feedback