Use VBScript in instruction files

If you want to use VBScript with <SOP> elements, the SOP parameters must be included in a hidden span (labeled
parameter1
) that contains the <SOP> element. At runtime the
eProcedure
Server replaces the <SOP> element with its value and the VBScript accesses the value by referencing
parameter1
.
In the VBScript, insert the element
<SOP>parameter1</SOP>
where
parameter1
is a legal parameter for this phase:
<FORM>
<SPAN id="Parameter1 style=display:none><SOP>PARAMETER1</SOP></SPAN>
<SCRIPT language=vbscript>
msgbox document.all("Parameter1").innertext
</SCRIPT>
</FORM>
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal