Search
FactoryTalk Energy Manager User Guide
Add Component
This section allows the users to add and configure various nodes (Region/Site/Area/Work Center/Work Unit). Refer to the
Create Energy Model
chapter.
Create Energy Model
Add Enterprise Node
Add Region Node
Add Site Node
Add Area Node
Add Work Center Node
Add Work Unit Node
Add Resource/Utility Meter
Add Production Meter
Add Process Value Meter
Add Virtual Meter
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.
Normal