Add Production Meter

Focuses on detailed production data. It helps track energy intensity within production processes, enabling managers to optimize production efficiency, reduce energy waste, and enhance overall productivity.
Perform the following steps to add the
Production
meter to the hierarchy list:
NOTE:
The following point is required to view data on
Production
meter dashboard:
  • Correct tag mapping should be done for production count measurement.
  1. Select
    Site
    or
    Area
    or
    Work Center
    , or
    Work Unit
    from the hierarchy list.
  2. Click the [] icon and click
    Add
    .
    Work Unit - Add
    User can also add the Production Meter from the Site Configuration page.
    Add Meter from Site
    The
    Add Component
    dialog box is displayed.
  3. Under
    Meter
    from the left pane, select
    Production
    and provide the following details:
    • Name
      : Provide a production meter name.
    • Description
      : Provide a description of the production meter.
  4. Click
    Add
    .
    Add Production Meter
    The "
    Added successfully
    " message is displayed.
    Production Meter Added
  5. To edit the details, refer to the Edit Component section.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal