Add Virtual Meter

Provides data from virtual meters, which aggregate information from multiple physical meters. This level allows monitoring and comprehensive analysis of energy usage across various segments, helping to identify trends and implement strategic energy management initiatives.
Perform the following steps to add a
Virtual Meter
to the hierarchy list:
  1. Select any Site or Area or Work Center or Work Unit from the hierarchy list.
  2. Click the [] icon and click
    Add
    .
    Work Unit - Add
    User can also add the Virtual Meter from the Site Configuration page.
    Add Meter from Site
    The
    Add Component
    dialog box is displayed.
  3. Under
    Meter
    from the left pane, select the
    Virtual Meter
    and provide the following details:
    • Resource/Utility Type
      : Select a resource type from the dropdown list.
    • Measurement
      : Select a measurement from the dropdown list.
    • Name
      : Provide a virtual meter name.
    • Description
      : Provide a description of the virtual meter.
  4. Click
    Add
    .
    Add Virtual Meter (Continued)
    The "
    Added successfully
    " message is displayed.
    Virtual Meter Added
  5. To edit the details, refer to the Edit Component section.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal