Configuring material lots
The
Lots
tab contains the information that identifies a particular
quantity of a material. A lot holds all of the static information about the lot, such as Lot
Identifier, Material Type, State of the lot, Engineering Units, and Controller ID value. A
lot may also contain sublots, which detail the actual quantity of the lot that is
distributed into material storage containers. An example of a lot could be: Shipment number
SN2009 of the material Granulated Sugar, which is part of the material class Sweetener and
is classified as a Raw
material type.Provide Feedback