Editing a lot
You can change the material’s properties and the amount of material in the lot, and distribute a lot of material to a container.
- From theEdit Materialdialog, select a record row to edit, and then click theEdit Lotbutton. TheEdit Lotdialog opens to theGeneraltab.

- Modify the general lot information as needed, and then clickApply.
- Select thePropertiestab. The properties assigned to the lot of material display. You can change the value of the property directly in theValuecolumn or use a form.

- In theValuebox, type a new value for the property.IMPORTANT:If you are changing a value that contains a decimal, use the Delete key to delete the value before typing a new value that contains a decimal. If you type over the old value containing the decimal, the new decimal is not recognized by the application.
- ClickApplyto save the changes, or clickOKto save the record and close the dialog box.
Provide Feedback