Using a form to change lot properties
- On thePropertiestab, select the record row to edit, and then click theEdit Propertybutton. TheEdit Lot Propertydialog opens.

- In theValuebox, type the value of the property, and then clickOK.IMPORTANT:If you are changing a value that contains a decimal, use the Delete key to delete the value before typing a new value that contains a decimal. If you type over the old value containing the decimal, the new decimal is not recognized by the application.
Provide Feedback