Distributing a lot
When you distribute a lot, you create a sublot that is identified by a label. A sublot is
an amount of material in the selected lot that is distributed to a container.
TIP:
Before creating distributions, verify that both the material lot and container have a
state of Ready to Use.
- From theEdit Lotdialog, select theStoragetab. Existing sublots display in ascending order by label name. Each record row represents a sublot. You can sort the list by clicking the column header to display an up arrow (ascending) or down arrow (descending).

- Select the record row to distribute, and then clickDistribute. TheDistribute Lotdialog opens.

- In theLabelbox, type a unique name for the sublot.
- In theQuantitybox, type the amount to distribute.
- From theStorage Containerlist, select a container to store the distributed amount.
- ClickOKto return to theStoragetab on theEdit Lotdialog.
- ClickApplyto save the changes, or clickOKto save the record and close the dialog.
Provide Feedback