Adding new lots

  1. From the
    Edit Material
    dialog, select the
    Lots
    tab. Existing lots display in ascending order by lot name. You can sort the list by clicking the column header to display an up arrow (ascending) or down arrow (descending).
  2. Click the
    New Lot
    button to insert a new lot record row.
    FTBMM_ED_odin_edit_material_lots
    The following is a list of items on the
    Lots
    tab:
    Lots items
    Item
    Description
    Lot Name
    Unique name to identify the lot (
    required
    ).
    State
    Current state of the lot (
    required
    ).
    Quantity
    Total amount of this lot of material (
    required
    ).
    Creation Date
    Date and time the lot was added (
    view-only
    ).
    Depletion Date
    Date and time the lot was deleted (
    view-only
    ).
    Controller ID
    Defaults to the next numeric value in sequence. You can change this to a unique number for PCD phase programming.
    Description
    Detailed description of the lot record.
    Refresh
    button
    Re-queries the materials database for lots of this material and repopulates the displayed lot records.
  3. Type the information in the appropriate boxes to define the material lot.
  4. Click
    Apply
    to save the changes, or click
    OK
    to save the record and close the dialog.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal