Changing a sublot quantity
- TIP: If you edit a sublot by distributing the lots of material, deleting a distribution, or changing the amountn of material, the material's inventory information also changes.From theEdit Lotdialog, select theStoragetab. The distributed amounts of the lot display.
- Select the record row to edit, then clickEdit Distribution.

- IMPORTANT: If you are changing a value that contains a decimal, use theDeletekey to delete the value before typing a new value that contains a decimal. If you type over the old value containing the decimal, the new decimal is not recognized by the application.Type a new amount in theQuantitybox.
- ClickOKto return to theStoragetab on theEdit Lotdialog.
- ClickApplyto save the changes, or clickOKto save the record and close the dialog.
Provide Feedback