Tree control (left pane in the RSWho)

The left pane of the
RSWho
is the tree control, which shows networks and devices.
The RSWho icon RSLinx Classic Linked Icons PNG FIle Template indicates a network. If the icon is animated, the network is being browsed. The RSWho only browses one network at a time. A network is browsed when you click the "+" sign to expand it, or select it or a device under the network node. When the network or device is collapsed (indicated by the + sign), click + or double-click the network or device icon next to the + to expand the view and begin browsing. When the network or device is expanded (indicated by the - sign), click - or double-click the network or device icon next to the - to collapse the view.
Right-click a supported device to select Station Diagnostics, Configure DDE Topic, or other supported services for that device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal