What does a red X in RSWho mean?

A red X in RSWho indicates that an error currently exists with a previously recognized node. The red X indicates a communication status error, such as unplugging a recognized device. For example, if Autobrowse is enabled, RSWho recognizes nodes during the browse cycle and stores the node information. During subsequent browse cycles, if an error occurs, such as a communication cable being pulled from a device, RSWho places a red X over the device to indicate that it cannot be recognized. Red X's will not appear if you are working in offline mode (Autobrowse is disabled or cleared).
To remove a red X from RSWho, right-click the node and select
Remove
.
TIP:
Removing a node from RSWho also removes all associated information, such as network shortcuts.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal