Remove a node in RSWho

In the RSWho Tree Control (left pane) or the List Control (right pane), right-click the node and select
Remove
.
To remove a node:
  1. In the RSWho tree control (left pane), right-click the node you want to remove and select
    Remove
    .
  2. Click
    Yes
    when prompted with, "Are you sure you want to remove this node?" The node is removed from the display.
    TIP:
    If Autobrowse is enabled, or if you click Refresh, the node will reappear on the next browse sequence. To remove multiple nodes, right-click the node that contains the nodes you want to remove and select Remove. This removes the node and all associated items.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal